6/14/2016 4:27 PM | |
Joined: 1/21/2013 Last visit: 11/20/2024 Posts: 4620 Rating:
|
Hello, LOGO! 0BA6 - 7 - 8? Have you already seen in the example? Or have you searched in the site Explorer above? LOGO! Application Examples - PLCs - Siemens some like this: Logo speed control - Entries - Forum - Industry Support - Siemens |
6/14/2016 5:59 PM | |
Joined: 12/18/2014 Last visit: 9/14/2025 Posts: 35960 Rating:
|
I hope I have understood you correctly. Then this would be a possible solution. AttachmentSpeed.zip (301 Downloads) |
6/16/2016 4:05 PM | |
Posts: 7 Rating:
|
Hi Dinos, thank you for your reaction. I have made a working diagram, hope it will clarify the way to a solution. |
6/17/2016 1:01 AM | |
Posts: 124 Rating:
|
Hello Kakiek, The timing diagram is very clear. I will work in that. See you |
6/17/2016 7:18 PM | |
Posts: 124 Rating:
|
Hello Kakiek. Attached a program to speed control. In the picture that you sent, we have four situations. 1. I considered buttons to start and stop. 2. For a time less 30 seconds, there is no way. Less then 30 seconds can be any time between zero to 30. I considered "More than 15 seconds" and maintained "More than 30 seconds". 3. Also there is a situation which the RL doesn´t change its state when the speed goes down and goes up during a interval less then 5 seconds. I maintained (third condition). Please take o look. May be something must be modified according your requeriments. I hope it helps you.
AttachmentKAKIEK 17 06 2016.zip (311 Downloads) |
Last edited by: Dinos at: 6/17/2016 7:19:52 PM |
|
Follow us on