9/6/2016 2:45 PM | |
Joined: 12/18/2014 Last visit: 9/14/2025 Posts: 35958 Rating:
|
Here is a simple example of the use the PI controller. I accepted as filling height 2m. 0V correspond in the example 2m filling height, the distance between sensor and liquid is the least. 10V correspond 0m, the distance between sensor and liquid is the greatest. With the switch at I1 of the controller is switched the PI Controller to automatic. The controller parameters (KC and TI) then you need to set yourself. AttachmentTank.zip (307 Downloads) |
This contribution was helpful to
1 thankful Users |
9/6/2016 3:46 PM | |
Joined: 10/10/2010 Last visit: 7/5/2025 Posts: 309 Rating:
|
is this program example has autotunning function ? |
Follow us on