10/13/2016 6:19 AM | |
Joined: 12/18/2014 Last visit: 9/11/2025 Posts: 35950 Rating:
|
The LOGO! 0BA8 can create a maximum of 16 connections. A maximum of 8 static and a maximum of 8 dynamic connections. The dynamic connections have the same "connection terminal". In the attached example you can see that 16 connections can be made. AttachmentProject_with_16_connections.zip (269 Downloads) |
Follow us on