(0)| 10/21/2016 12:20 AM | |
|
Joined: 9/3/2014 Last visit: 2/13/2025 Posts: 79 Rating:
|
Dear experts, I'm working in a automation project, which one consists in a technology migration, we need to replace 4 simovert inverters and we have bought Sinamics g120 inverters, each motor have a resolver, the frecuency of this is 10 Khz, the voltaje is 5,5V and the poles number is 4, about the motor information, the voltage is 380V, nominal speed: 3000 rpm and nominal frecuency 100 Hz. The issue is that we don't know if the CU250S is able to read the resolver signal, we are not sure if the frecuency is in range of CU250S. Phisically we can connect the sensor to the CU250S, the same connections that in the Simovert inverter. We will be grateful if you can help us. Thanks in advance. Andrés Felipe Ariza Attachmentresolver.pdf (287 Downloads) |
| 10/27/2016 1:52 PM | |
|
Posts: 1410 Rating:
|
A HTL has usualy only one wire per channel 24V: |
Follow us on