11/3/2016 4:11 PM | |
Posts: 52 Rating:
|
Hello When I open the project the software that is missing is DRIVE ES. In another projects when this was a problem I just installed STARTER and this was no problem anymore. The new project has the same software requirement, but when install starter (V4.5) i get this message again. When I make execute the problem disappeared and i could open the project without any warnings. I tried to copy this program to and open it in Simatic Manager, and the same software requirement. Is this the solution (to make execute) or should i try something else. Best regards. Deco10 AttachmentDrive ES.zip (358 Downloads) |
11/3/2016 4:18 PM | |
Joined: 5/12/2006 Last visit: 9/2/2025 Posts: 22709 Rating:
|
Hello, you can also try to make a "Save as" with reorgisation if then the message dissapear. Regards Christoph |
Follow us on