(0)| 12/4/2016 4:02 AM | |
|
Joined: 10/13/2013 Last visit: 10/8/2025 Posts: 6 Rating:
|
Hello my friend. I am currently programming a v90 PN: I have problems with the telegram on the siemens page there is an example with telegram 3. but this one does not recommend, the one they mention that should be used is 5 or 105. Have some examples with these recommended telegrams. Even your message is in your last comment. I need your help.
------------------------------------------------------------------------------------------ |
Last edited by: doloemanuel at: 12/4/2016 4:07:03 AMLast edited by: Min_Moderator at: 12/5/2016 12:59:44 PMNew subject after splitting Last edited by: Min_Moderator at: 12/5/2016 1:01:47 PM |
|
| 12/4/2016 5:21 AM | |
|
Posts: 8092 Rating:
|
Hello doloemanuel, Extracts from the manual - about V 90 PN standard telegrams are as below. The standard telegram 1 can be used only for RT mode. The standard telegram 2, the standard telegram 3 and the Siemens telegram 102 can be used either for RT mode or IRT mode depending on the IO controller. The standard telegram 5 and the Siemens telegram 105 can only support IRT mode. The standard telegram 1 (RT mode) and the standard telegram 2 (IRT mode) will be used in this basic application. So what problem do you face? which is the controller? For application examples, visit this Sinamics V-90 PN examples page & read different applications. HTH. |
Follow us on