(0)| 12/12/2016 5:50 PM | |
|
Joined: 9/27/2006 Last visit: 1/20/2026 Posts: 12481 Rating:
|
Hello Nachate; As you will see from the following extract, the answer to your quetion will depend on the type of panel you wish to donload to. The best way for you to get an answer is to download the specific manual for your panel; search for it using the Search Box at the right of this page. SIMATIC HMI WinCC flexible 2008 WinCC flexible 2008 Compact/ Standard/ Advancedhttps://support.industry.siemens.com/cs/fr/en/view/18796010/1457820811
Transfer modes Depending on the HMI device, you can use one or more of the following transfer modes: · Direct connection (USB cable (host-to-host), serial cable) Transfer takes place by means of a serial cable or a USB cable connecting the configuration computer and HMI device. · Ethernet network connection The configuration computer and HMI device are located in a network or are connected point-to-point. The transfer operation between the configuration computer and the HMI device takes place by means of an Ethernet connection. · MPI/DP The configuration computer and HMI device are in an MPI network or PROFIBUS DP network. The corresponding protocol is used for the transfer operation. · Http Transfers are based on the http protocol, for example via Intranet or
Internet. ·
File · S7Ethernet The configuration computer and HMI device are located in a network or are connected point-to-point. The transfer operation between the configuration computer and the HMI device takes place by means of an Ethernet connection. S7Ethernet is transfer channel that can be used for routing. Routing is only supported for integrated operation of WinCC flexible in STEP7. The configuration computer/HMI device are connected to one of the following networks: · - MPI · - PROFIBUS DP · - Ethernet · The transfer mode setting for an HMI device is also applied if the HMI device is selected in the project view and one of the commands on the "Project > Transfer" menu is selected (for example, in the case of a back transfer operation or when the operating system is updated on the HMI device). · Transfer to the OP 73micro, TP 170micro, TP 177micro, OP 73, OP 77A and TP 177A HMIs· The "RS 232 / PPI Multi Master Cable" (6ES7 901-3CB30-0XA0) serial cable is required to transfer project data to the OP 73micro, TP 170micro, TP 177micro, OP 73, OP 77A and TP 177A HMIs. It is imperative that DIL switch 5 is set to 0. · Only serial transfer is possible at micro operating panels. All other HMIs support either serial data transfer or MPI transfer. By changing the transfer mode of a channel in the transfer settings, you disable the corresponding other channel.
· OP 73, OP 77A and TP 177A HMIs do not support simultaneous data transfer via MPI from several active instances of WinCC flexible to multiple HMIs. These devices only execute the initial first transfer request. Hope this helps, Daniel Chartier
|
| 12/13/2016 12:04 PM | |
|
Joined: 8/3/2009 Last visit: 1/21/2026 Posts: 16653 Rating:
|
Hello NACHATE As in understood you want to get the Project from the Panel? This is a little Problem because the Project files are not on every Panel. There are in almost 99% only the Runtime Files on the Panel. The only Way to do this is to use the Backtransfer Option. But someone had to loaded up the Project on the Panel that you can use it: https://support.industry.siemens.com/cs/ww/en/view/21907703 If It doesn´t work you have to get the Project Files from the machine manufacturer. Bye Murof |
|
If this Information really helps, you could use the Rate function |
|
Follow us on