10/20/2011 8:56 AM | |
Posts: 739 Rating:
|
F0070 “CB setpoint fault” is a watchdog failure. For information pls. see FAQ: What are the possible causes of F0070 on MICROMASTER 4, and how do I avoid them? http://support.automation.siemens.com/WW/view/en/22329309 Pls have also a look into p2014 and p2040 |
This contribution was helpful to
1 thankful Users |
10/20/2011 9:23 AM | |
Posts: 241 Rating:
|
p2014 and p2040 has already set to 3000ms... And LED goes to green... |
12/22/2016 12:23 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4760 Rating:
|
New question published by theoulis7 is split to a separate thread with the subject MM440, fault F0070 when reaching max frequency. Best regards |
Follow us on