4/28/2008 8:05 AM | |
Posts: 53 Rating:
|
Hi, Im using for process control PLC S7 314C-2DP with OPC Server (Siemens) to provide data for HMI. My problem is that i cant watch online more then one FB/FC/VAT. Cant even use VAT for set/force variable (only way is to turn off online monitoring, set variable and then turn on online monitoring). So my questions are: 1. There is any chance to change it ? (do some changes in configuration or it is limited by PLC...I had never problem like this on PLCs S7 4xx) 2. What kind of communication are used for online watching FB/FC/VAT ? (S7 communication or ... ?) In attachment is my S7 Project (without blocks) to check configuration. Best regards. Henio. AttachmentCpu314c.zip (535 Downloads) |
5/5/2008 5:19 PM | |
Joined: 9/23/2005 Last visit: 9/10/2025 Posts: 4416 Rating:
|
Hi, the number of breakpoints stay on FAQ http://support.automation.siemens.com/BR/view/pt/22725914 |
Denilson Pegaia |
|
Follow us on