1/27/2017 10:55 AM | |
Joined: 4/28/2009 Last visit: 6/3/2025 Posts: 347 Rating:
|
Hello, did you try flying restart function? With regards |
1/27/2017 11:24 AM | |
Joined: 7/2/2010 Last visit: 5/9/2025 Posts: 53 Rating:
|
Hello ! This is the first thing in my mind to apply but i am not sure if it works when the motor is rotating in reverse. |
1/27/2017 11:45 AM | |
Joined: 4/28/2009 Last visit: 6/3/2025 Posts: 347 Rating:
|
Hello, yes, it is possible to start motor to other direction than it rotate. See attached part of commissioning manual. Now I'm not sure which setting of p1200 will be best for this case, in manual there is p1200 = 1 to 3 for search in both directions. With regards Attachmentmm flying restart.pdf (439 Downloads) |
Follow us on