3/25/2017 10:32 PM | |
Joined: 11/17/2010 Last visit: 9/12/2024 Posts: 216 Rating:
|
Hi, You have 2 ways to force screen : 1 -From PLC : Declare Job mailbox area in Connexion menu and force screen from PLC using function number #51 according to IO adress bit value. 2 - From HMI: - Create a tag who is linked to your PLC IO bit (MyTag). - Create a script in which you test MyTag to 1 (ForceScreen()) :
- Into Tag table -> Click on MyTag -> Go to Events tab -> Under Change value, click on Drop down box and select VB functions ChangeScreen. Regards. AttachmentHMI-Area pointer-Job Mailbox.pdf (249 Downloads) |
This contribution was helpful to
1 thankful Users |
3/27/2017 4:59 AM | |
Joined: 5/1/2013 Last visit: 1/22/2025 Posts: 428 Rating:
|
Thank you but where can I find that menu ... I am using step7 5.5 and tia wincc v13 |
3/27/2017 11:00 AM | |
Joined: 8/3/2009 Last visit: 9/18/2025 Posts: 16452 Rating:
|
Hello RetroK Here is the official FAQ to this Topic: https://support.industry.siemens.com/cs/ww/en/view/93909293 Bye Murof |
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to
1 thankful Users |
3/27/2017 11:31 AM | |
Joined: 11/17/2010 Last visit: 9/12/2024 Posts: 216 Rating:
|
Hi Murof, I thought about the second option of the FAQ but, when value change from 1 to 0, Event is trigged again and screen is displayed again. RetroK want tp show screen only if IO bit turn ON. Regads |
Last edited by: Panov69 at: 3/27/2017 11:32:17 AM |
|
This contribution was helpful to
1 thankful Users |
Follow us on