4/25/2017 4:27 AM | |
Posts: 2 Rating:
|
Hola amigo, oye me podrias auxiliar en la programacion para arrancar un motor, ya configure toda la red profibus, pero tengo problemas con las palabras de mando y la funcion move, me podrias ayudar? -------------------------------------------------------------------- Hi friend, hey you could help me in programming to start an engine, and configure the entire profibus network, but I have problems with the command words and the move function, could you help me? ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 4/25/2017 11:24:23 AMTranslation Last edited by: Min_Moderator at: 4/25/2017 11:25:24 AMNew subject after splitting |
|
4/25/2017 11:53 AM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4760 Rating:
|
Closed cause question published twice. The second thread with the subject Control an MM4 drive from the S7-300 PLC is located within the MICROMASTER conference. Best regards |
Follow us on