(2)| 6/1/2017 9:44 PM | |
|
Posts: 623 Rating:
|
Hi mugurelgi5, AND M40.1 with i1,0 at the EN parameter. This will disable unscale block if M40.1 is low. Also Move 0 to PQW directly if M40.1 is low. |
This contribution was helpful to
|
|
| 6/1/2017 11:22 PM | |
|
Joined: 5/30/2013 Last visit: 12/28/2025 Posts: 112 Rating:
|
Hi mugurelg5, 1) why are you have used MD31 and MD 55 2) if you wont initialize some value (Q- in this case) have used OB100 when start up. In this post you see how standardize and destarndardize analog values and calculated the output value. How can you standardize and destandardize analog values with STEP 7 V5.5? For an S7-1200/S7-1500 controller in STEP 7 (TIA Portal), how do you scale integer values in real numbers and vice versa for analog inputs and outputs? 3) if marker 40.1 "HIGH" or "LOW" which value wont in PQW304? 4) "I need the output value of FC106 to work intermittently". What does that mean exactly? Which time interval (second, minute, hour, day). For time response depend answer for the question. .Best regards zzVss |
Follow us on