6/29/2017 8:02 AM | |
Posts: 1 Rating:
|
Dear All, In my application the control unit cu240e-2dp for the sinamics G120,PM 240 45kw. The Dc link voltage 660 Vdc. Input supply 420 V ac. The problem is high dc link voltage,Connected resistor heating.Could anyone help to solve the problem. Is this is the issue of Braking Chopper ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 6/29/2017 2:28:20 PMNew subject after splitting |
|
7/1/2017 8:04 AM | |
Joined: 9/12/2016 Last visit: 6/26/2022 Posts: 17 Rating:
|
|
Follow us on