9/9/2008 2:03 PM | |
Joined: 3/29/2006 Last visit: 5/29/2017 Posts: 151 Rating:
|
See http://support.automation.siemens.com/WW/view/en/19562445 The fault is described in Masterdrives Compendium MC V2.4 and CUVC V3.4 OBS.: The work-around in the fault-list is not 100% correct. You cannot increase the "sign-of-life"-signal. This note is mixed up with F152. The "sign-of-life"-signal of F152 is created by a funtion-bloc in MC to monitor the Profibus-signals and has nothing to do with DriveMonitor. |
This contribution was helpful to
1 thankful Users |
2/21/2015 1:51 AM | |
Joined: 6/4/2008 Last visit: 8/5/2025 Posts: 1518 Rating:
|
Hi F152 - Signs of life repeatedly invalid See Function Diagram 170 Regards, Graeme |
2/23/2015 8:51 AM | |
Posts: 61 Rating:
|
Hi İ knew it but it is not enough for solution this problem |
Follow us on