7/27/2017 9:18 PM | |
Joined: 4/19/2013 Last visit: 9/8/2025 Posts: 61 Rating:
|
Dear All, Thank you all for the help. We already have answer for the solution in ( https://support.industry.siemens.com/tf/WW/en/posts/calling-sfc21-in-scl/3911?page=0&pageSize=10 ) But, I was not able to understand how can in use it in instantaneous DB which is made from UDT. e.g. VAR_TEMP END_VAR VAR FlushStationPipeData : PipeData; FILL(BVAL := Emptybyte // IN: ANY ; But this is giving an error as attached. Please do guide where I am going wrong. I had tried using DB address as p#DB1300.dbx110.0 byte 29 But it did not work in that case as well. Regards, Prayag Jaliahal |
Follow us on