10/3/2017 8:25 AM | |
Posts: 1 Rating:
|
Hello im working with Espiral so ill give some more details. We are using the seimens s7-1200 AC/DC/Rly connected to a incremental encoder from ifm (RA3100). The main issue is that when using the HSC we can only count up in units of two and are unable to count back down. We are using HSC_2 (enabled) using the following settings: Type of Counting: Count Operating Phase: A/B counter fourfold Initial Counting Direction: Count Up Clock generator A Input: %I0.2 Clock generator B Input: %I0.3 If you have any advice or links that could help us out it would be greatly appreciated. The Manual for the encoder can be seen in the attachment. Attachmentencoder.pdf (321 Downloads) |
Last edited by: Jen_Moderator at: 10/4/2017 11:39:43 AMNew subject after splitting Last edited by: Jen_Moderator at: 10/18/2017 12:14:50 PMMoved post back to this topic. |
|
Follow us on