10/12/2017 10:19 AM | |
Posts: 33 Rating:
|
Forcing DI signal. If a force job is active already, the variables together with the corresponding force values are displayed in bold face and the line in the identifier column is marked with the symbol. If the symbol is displayed, it indicates that the address is in part forced. So my question, does it also displayed the force signal in the actual DI module or it needs 24vdc supply of the force signal? Thanks for reply. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 10/13/2017 9:26:18 AMNew subject after splitting |
|
Follow us on