7/6/2008 11:57 AM | |
Joined: 11/8/2005 Last visit: 6/5/2024 Posts: 335 Rating:
|
Does SFC work with STEP7 v5.4 without installing PCS7? |
7/6/2008 3:35 PM | |
Joined: 9/27/2006 Last visit: 9/4/2025 Posts: 12397 Rating:
|
Hello SM; PCS7 uses a comination of SFC/CFC as engineering tools on the AS (SCL required in the background). Although CFC is offered as a Step 7 engineering tool, SFC is not. The standard stand-alone SFC tool for Step 7 (outside of PCS7 ) is named S7-Graph . you will find more information about it here: https://mall.automation.siemens.com/WW/guest/index.asp?nodeID=5000144&lang=en S7-Graph isone of the 5 PLC languagesof IEC 61131-3; as such, it differs from the PCS7 implementation of SFC. I have used it in different applications, and I find it very useful for sequential systems. Siemens offers S7-Graph also as part of its Step 7 Professional offering (Step 7 Basis + SCL + S7-Graph + S7-PLCSim). See here: https://mall.automation.siemens.com/WW/guest/index.asp?nodeID=5000906&lang=en Hope this helps, Daniel Chartier |
7/7/2008 1:01 PM | |
Joined: 4/23/2007 Last visit: 12/30/2024 Posts: 58 Rating:
|
Course it works...im using it atm |
"There is no spoon." |
|
Follow us on