12/4/2017 11:44 AM | |
Joined: 10/11/2006 Last visit: 9/5/2025 Posts: 6038 Rating:
|
Hello,the enable command following your enquiry, using analoque Axis with SIMOTION C240. Drifting is only possible when the enable output-Signal is True. Please have a look to the output signal if the connection comes from X2 . You also can make a Trace TO-Axis .control Attached file is a screenshot from Manual C240 X2 AttachmentC2xx_X2.pdf (406 Downloads) |
With best regards, |
|
Follow us on