(1)| 3/10/2018 5:28 AM | |
|
Posts: 8092 Rating:
|
Hello, If you are able to communicate with S7 PLC then try below point. On PC, in Starter set PG/PC interface as Ethernet, select device unit DCM, set / click on PG/PC as only master on bus, & check. OR If your PC has serial port you can establish communication via serial port. But it won't work with USB to serial converters & AOP30 must not be connected to drive. Please refer attached sheet for serial interface. HTH. Attachment6RA80 STARTER serial communication.pdf (578 Downloads) |
Last edited by: PISCEAN 2010 at: 3/10/2018 5:36:19 AM |
|
| 3/14/2018 7:22 AM | |
|
Posts: 69 Rating:
|
How to communicate PLC and DCM for encoder feedback? |
| 3/15/2018 5:57 AM | |
|
Posts: 8092 Rating:
|
Could you please explain your requirement in details? e.g. what you want to achieve? |
| 3/15/2018 11:52 AM | |
|
Posts: 8092 Rating:
|
Please refer SINAMICS DCC: Positioning and synchronism with SINAMICS DCM and CU320-2 example. |
Last edited by: Jen_Moderator at: 3/15/2018 1:33:54 PMOptimized link. |
|
| 3/15/2018 1:14 PM | |
|
Posts: 69 Rating:
|
CU320-2 is an additional module to be added ? |
| 3/16/2018 6:23 AM | |
|
Posts: 8092 Rating:
|
In this application, CU320 acts as technology CU & controls the application. Please refer Motion Control Applications with SINAMICS DCM 05/2017 (1,7 MB) document. |
Last edited by: Jen_Moderator at: 3/16/2018 10:15:25 AMOptimized link. |
|
| 3/16/2018 6:03 PM | |
|
Posts: 69 Rating:
|
Yea I have referred the pdf. So can't I control the drive with position feedback without this CU320 board? |
| 3/17/2018 5:58 AM | |
|
Posts: 8092 Rating:
|
Yes, & without advance CUD inSinamics DCM. |
| 3/19/2018 12:51 PM | |
|
Posts: 69 Rating:
|
How to do that without CU320? |
Follow us on