3/31/2018 5:11 PM | |
Posts: 16 Rating:
|
Dear All, We have a Siemens Master drive MC 6se7022EP50. There was a issue with the motor after replacing it. The Resolver value doesnt change. Do i have to something in the drive monitor after replacing it. The reollver value is connected from the analog out put of the drive. to the plc. Note : this was working before only after replacing the motor .we are facing issues.I have attached the diagram and drive monitor back up. Please help AttachmentMasterdrive.zip (316 Downloads) |
4/8/2018 12:52 PM | |
Joined: 4/23/2010 Last visit: 11/23/2024 Posts: 8092 Rating:
|
Hello plckid, Please check/refer the encoder interface & try by replacing inetrfacing module.
|
Follow us on