7/3/2018 10:42 AM | |
Joined: 11/29/2014 Last visit: 9/13/2024 Posts: 96 Rating:
|
Dear Experts, We have PCS7 7.0 SP3 redundant server with 5 os client and customized PCS7 metal library. We are facing issue in one of our os client pc. We are not able to see Interlock text in faceplate. We are facing this issue in only one client pc rest of 4 client pc are working ok.. Please find attached screenshot of faceplate of two os client. Is there any way to resolve this issue. Thanks & Regards, Dhaval Abotiyawala +919033161781 AttachmentFaceplate.zip (139 Downloads) |
7/3/2018 11:06 AM | |
Joined: 3/14/2008 Last visit: 9/4/2025 Posts: 2216 Rating:
|
Since it is a custom faceplate,I cannot direct you to the root cause, but can you copy the associated faceplate files from the working client to the non working client? I think the client with the problem does not have the correct faceplate file? |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to
1 thankful Users |
Follow us on