(0)| 9/6/2018 2:10 PM | |
|
Posts: 68 Rating:
|
Hi Everyone, I faced problems while uploading program from "IM151 - 8 PN/DP". I uploaded the program in the backup in online, by "Upload to PG" Option. Even after uploading the program from the PLC, i had difference between Online / Offline Projects. Then i faced error while editing the logic in the online PLC, i have received an error "The memory space in the module is not sufficient. Do you want to compress the Load Memory". I proceed with "Yes" Option for that error. But still i faced the same issue. I cant able to reset the PLC through "Simatic Manager -> IM151-8 CPU -> PLC -> Clear/Reset" option, then i restarted the CPU. Still the program is present in the CPU. When i tried with "Simatic Manager -> PLC -> Compile and Download Objects " i downloaded the modified backup. Then the same memory insufficient problem is occurring when i modify the online programming. I have attached the error i faced regarding this issue. Please give me have a solution for this problem.. AttachmentError.docx (160 Downloads) |
Follow us on