(0)| 8/4/2018 4:23 PM | |
|
Posts: 22 Rating:
|
today i get the diagnostics but i found the below event and repeated more than 15 time which is: Event 2 of 120: Event ID 16# 73A3 DP: loss of redundancy at DP slave Address of affected DP slave: station number: 7 DP master system ID: 2 Log. base address of the DP slaves: Input address: 16365 Log. base address of the DP master: Input address: 16375 Requested OB: I/O redundancy error OB (OB70) Priority class: 24 Incoming event 07:50:06.757 PM 08/01/2018 (Coding: 16# 73A3 1846 C054 3FF7 3FED 0207) Also the A/M event affected more than DP slave station (attached diagnostic) AttachmentDiagnose2.8.2018.txt (418 Downloads) |
Follow us on