10/4/2018 10:46 AM | |
Posts: 6 Rating:
|
Hi, Application is Unwinder, Slitter, Rewinder in Pulp and paper industry Our hardware config is as follows: CPU 1516T-3 PN/DP (1 No): 6ES7 516-3TN00-0AB0 MASTERDRIVES (5 Nos): Simovert MasterDrives VC (CUVC) CBP2: 6SE7090-0xx84-0FF0/0FF5: . FRABA Encoder (3 Nos): OCD-DPB1B Drives and encoders are connected on profibus. My question is do we have standard library to do the Unwinder, Rewinder application using Simovert masterdrives as like this one (but it uses Sinamics VFDs). If not... is it possible to convert . achieve functionality of this library somehow using simovert masterdrives ? or if not... then what I should do to deliver winder and unwinder standard functions using S7-1500T and Simovert masterdrives in a standard manner, because commissioning time and budget is not great to sit and R&D on things. |
Last edited by: pwade at: 10/4/2018 10:48:21 AM |
|
10/9/2018 11:01 AM | |
Joined: 10/11/2006 Last visit: 9/15/2025 Posts: 6040 Rating:
|
Hello, it is not possible to convert the "DCC winder" to Masterdrives. A similar functionality was available with the T400 option board with winder software 6DD1842-0AA1 - but this product is, like Masterdrives, already discontinued. A basic winder application using free blocks had only a reduced functionality compared to the "DCC winder" and was discontinued as well and you would not get support for it anymore. We would recommend to use the winder application for S7-1500(T). |
With best regards, |
|
Follow us on