10/2/2018 10:29 AM | |
Joined: 10/29/2015 Last visit: 9/19/2024 Posts: 182 Rating:
|
Hi, by creating /etc/sysconfig/network/ifcfg-eth0 on a Gentoo-Linux I got LSC 8.2 working. Thanks for this hint. However another Gentoo still fails and I have no idea why. The main interface is also eth0, so I created that empty file. Now I get "java.lang.UnsupportedOperationExeption: adapter type is not support" just like mentioned this other thread. I see there are more interfaces available like wlo1 and vmnet1, but which are not used. Anyway I created those empty files as well. Now I get "java.lang.UnsatisfiedLinkError: /usr/lib64/rxtx-2/librxtxSerial-2.2pre1.so: /usr/lib64/rxtx-2/librxtxSerial-2.2pre1.so: undefined symbol: minor" But linking looks fine here:
------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 10/2/2018 10:40:46 AMNew subject after splitting Last edited by: massb at: 10/2/2018 11:45:11 AMLast edited by: massb at: 10/2/2018 11:47:28 AM |
|
Follow us on