11/13/2018 2:53 PM | |
Joined: 8/3/2009 Last visit: 9/11/2025 Posts: 16400 Rating:
|
Hello RoboKD Why do you want to go online with?? the Panels have no Online Diagnostic functions.... If you want to load the Project to the Panel or do something else then you have to get sure that the Ports you are using are not blocked. The used Ports you will find at: https://support.industry.siemens.com/cs/de/en/view/109755202/105572859275 Bye Murof |
If this Information really helps, you could use the Rate function |
|
11/13/2018 3:11 PM | |
Joined: 6/27/2017 Last visit: 3/29/2023 Posts: 2 Rating:
|
If I am on the local machine network, I can go online with the panel and open the runtime and monitor/control the cell. I wanted to be able to do this from the plant side of the S602, I currently have all ports open the TP1200. It seems that I need to use Sm@rtserver to do this. |
Follow us on