12/20/2018 8:45 AM | |
Posts: 6 Rating:
|
Brilliant, thankyou. that has worked and i am now online with the plc, i am having one more issue with the HMI and the already loaded program which was created with v15 i can connect to the HMI fine, but when i try to download the new programe on the HMI it appears to time out after a min or so and comes up with a connection error. any ideas how i could remedy this so i can wipe the old v15 program, and download the new v13 prog ?
------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 12/20/2018 2:13:21 PMNew subject after splitting |
|
12/20/2018 9:45 AM | |
Joined: 5/12/2006 Last visit: 9/15/2025 Posts: 22710 Rating:
|
Hello, try to use prosave to reset the panel and downgrad to the old v13 FW.
Christoph |
Follow us on