1/15/2019 11:10 AM | |
Joined: 6/4/2008 Last visit: 7/25/2024 Posts: 30 Rating:
|
Hello i have a problem with a s5 system with four cpus and a coocrdinator.Almost every two days all cpus go to stop and the first cpu needs overall reset.I checked the back up programm from all cpus with the online and i dont see differences.I changed the main psu, all cpus coordinator and the rack but still the problem occurs.Because this problem occurs at night shift( i work in the morning) i couldnt check the i stack every time.The only time i could check i got these screens and i couldnt find out what the problem is.I would appreciate any help thank you in advance Attachmentistack.zip (422 Downloads) |
Follow us on