(0)| 2/15/2019 9:44 PM | |
|
Posts: 4 Rating:
|
I have a just installed a Sinamics V20 to replace a a different model VFD. It is up and running but I need to get a 120v run signal to a PLC. I thought I could use the DO2 but when I checked continuity on the N.C. relay it is energized rather the unit is running or not.and the N.O. never shows continuity. Is it possible to get a 120v source with the unit running that terminates when the unit is stopped. Is the relay programmable. ------------------------------------------------------------------------------------------ |
Last edited by: AutoGen_681769 at: 2/15/2019 9:48:09 PMLast edited by: Jen_Moderator at: 2/18/2019 7:13:40 AMNew subject after splitting |
|
| 2/18/2019 8:47 PM | |
|
Posts: 4 Rating:
|
What value would go in P0732 for bit 02 in r0052. I must be missing something. You're probably regretting answering this post but I do appriciate it |
| 2/19/2019 6:27 PM | |
|
Posts: 4 Rating:
|
Thank you very much for your assistance. We have it up and running and it is doing just what we want. Thanks again |
Follow us on