2/15/2019 10:59 AM | |
Posts: 3 Rating:
|
My logo is new and is a 6ED1052-1MD08-0BA0 with a AM2 module. I only use 1 output q1. And the example of faq 24003057 is the only program in my logo. Ax is a Pt100 4-20mA on AI1 and Ay is a fix signal AM1 set by the web editor. When I program' for example, a on threshold of 10 and a off threshold of 5, the comparator works well, BUT the output q1 flips multiple times on-off the moment that Ax-Ay go's over from 1 to -1 and visa versa. With a on threshold of 2 and a off threshold of -2, the output q1 flips multiple times on-off the moment that Ax-Ay go's over from 1 to -1 and visa versa. AttachmentbranderregelingV2.zip (183 Downloads) |
Last edited by: Bart Lauwers at: 2/18/2019 8:18:52 AM |
|
2/15/2019 11:03 AM | |
Joined: 12/18/2014 Last visit: 9/10/2025 Posts: 35946 Rating:
|
Can you upload your program as an Zip file? Which range has the are the 4-20 mA? 0-100 °C or another range? |
2/18/2019 8:22 AM | |
Posts: 3 Rating:
|
Peter, i will check my grounding of the power supply. I also uploaded my program in a zip file. |
2/18/2019 8:24 AM | |
Posts: 3 Rating:
|
Iox65, i have uploaded my program in a zip file. |
Follow us on