2/28/2019 9:39 PM | |
Posts: 2 Rating:
|
Hello, almost four years later, your diagram is excellent. The value of B007 is correct. But, I want an infinite counter, like an odometer (which measures the kilometers that your car travels without reset). I mean, QUESTION: I can "initialize" my counter when the program START runs by setting the value of B007. The problem is in third day. For example: DAY#1 = 10 YESTERDAY = 0, DAY#2 = 5 YESTERDAY = 10, DAY#3 = 20 YESTERDAY = 5 (has to be 15) but I want my counter accumulate TOTAL counts (TOTAL = 15 + 20 = 35). It's possible? I have models LOGO! 8.FS4 ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 3/1/2019 7:02:38 AMNew subject after splitting |
|
2/28/2019 10:16 PM | |
Joined: 12/18/2014 Last visit: 9/10/2025 Posts: 35947 Rating:
|
Hello carlos.granadeno, at first welcome to the forum. That's possible. See attachment. AttachmentCounts_FS4.zip (185 Downloads) |
This contribution was helpful to
1 thankful Users |
Follow us on