5/8/2019 4:52 PM | |
Posts: 1 Rating:
|
I'm working with SIPROTEC 7SD522. After going online with a parameter file having a version number V4.73 and initializing the 7SD522 device several times while trying different things etc every thing was working well. Then I decided to download a project with a parameter file having a version V4.73 without updated the parameter file to V4.7. I managed to initialize the device and download into the 7SD522 successful and without any apparent problems. On trying to initialize again with some other projects ( the ones that I was working before) I start having the below massage and unable to initialize the 7SD522 any further. Any suggestions please? We have also tried below suggestion of putting off the under voltage protection under tagging with no success. Your assistance will be highly appreciated. ------------------------------------------------------------------------------------------ AttachmentErrorBuf.txt (373 Downloads) |
Last edited by: Jen_Moderator at: 05/09/2019 10:59:56New subject after splitting |
|
Follow us on