5/8/2019 5:45 PM | |
Posts: 3 Rating:
|
Hi, I first thought it will be Ok to use the 6ES5955-3LC41 on the 6ES5155-3UA11 Central Rack because they have the same connectors (8-pin for 5 V and 37-pin for control signals), but doubts emerge when you take a look at the pin configuration (see PDF attached) which was taken from Siemens System Manuals: - In 6ES5955-3LC41 8-Pin connector, pins 4 to 6 do not exist. I don't know if that would be relevant at the 3UA11 Central Rack - In 6ES5955-3LC41 37-pin connector, pin 6 doesn't show function HOLD and pin 26 doesn't show function RLSA. Also pins 34-35 are not assigned -15 V. Are these just type errors in the pictures? Thanks in adnace for your next feedback AttachmentS5 Power Supply Connector Comparison.pdf (662 Downloads) |
Follow us on