9/11/2019 11:05 AM | |
Joined: 10/10/2005 Last visit: 1/29/2025 Posts: 1940 Rating:
|
Hello Khangtd46, I think this is a substitute product.A substitute product is compatible with the previous product. This means that it supports all the functions of the previous product and might also have additional functions. In this case it is possible to replace the previous product with the substitute product with having to reconfigure. See also the informations of the FAQ: With best regards |
This contribution was helpful to
1 thankful Users |
Follow us on