1/20/2020 3:50 AM | |
Joined: 1/5/2017 Last visit: 8/7/2025 Posts: 2 Rating:
|
Hi Guys, Working with an S5 115U PLC, getting a lot of PLC Stops randomly. See attached photos for iStack info. I am trying to work out what is causing the stop, any help would be appreciated. I see that STOANZ indicates an internal stop request, so I assume this is a STP instruction, could it also be from an STS instruction? Currently get a STOANZ fault on the iStack info and it indicates the areas of the program below. The weird thing is if we get a PLC stop, flicking the PLC switch from run to stop and back does nothing, but if we power cycle the power supply to the remote IO rack and then try it works. The power supply has been swapped with another and the issue persists. Any ideas on what to look for? [snip] ... AttachmentPicture.zip (395 Downloads) |
Last edited by: CS Moderator at: 01/20/2020 10:20:15Pictures attached |
|
1/20/2020 9:54 PM | |
Joined: 12/18/2014 Last visit: 9/17/2025 Posts: 35967 Rating:
|
No, you must know, at which address and in which block the CPU goes to STOP. For error 0334: "System message no. 0334" when attempting to go online with STEP 5 V7.2 in Windows XP |
Follow us on