2/20/2020 12:03 AM | |
Joined: 9/27/2006 Last visit: 9/10/2025 Posts: 12405 Rating:
|
Hello siemeneitor; Have a look at this thread which discusses the same issues you are asking about: Step 5 is the official Siemens program for the S5 family, but it runs under DOS (or a Command window, up to WIN XP), and is now considered obsolete. An alternative could be this product from IBH Softech, it runs under Windows: https://www.ibhsoftec.com/epages/63444704.mobile/en_GB/?ObjectPath=/Shops/63444704/Products/10018 They also offer programming cables designed for newer Windows OS. Hope this helps, |
Last edited by: dchartier at: 02/20/2020 00:09:21 |
|
2/20/2020 12:21 AM | |
Posts: 10 Rating:
|
Thanks Dchartier, your answer was very helpful. That software looks very reliable and better than S5 on MS-DOS, do you have any experience using it? i read that it can be used for upload, download and editing programs. |
Follow us on