(0)| 6/1/2020 9:04 AM | |
|
Posts: 413 Rating:
|
How can i check thePCMCIA card (6FC5247-0AA11-0AA1) - is the card healthy or not?? What program can do it? I have SIMATIC FIELD PG M2 (6ES7713-1BB10-0AC1) there is a card reader...(from the left side), I tried using Sinucom FFS (v01.00.03) but I do not understand in the settings of this program need to choose Addition.programs - Reaer - what should be there? do i need a program CardWare? Where can I download it? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 06/02/2020 06:42:10New subject after splitting |
|
| 6/2/2020 6:49 AM | |
|
Posts: 8171 Rating:
|
Closed cause question posted twice. The second thread with the subject 840D - can not reset! Sos! is published within the conference SINUMERIK CNC automation systems.
|
Follow us on