12/21/2008 12:20 PM | |
Joined: 9/27/2006 Last visit: 9/10/2025 Posts: 12405 Rating:
|
Hello Abod; I f you look at the following attached document, you will see that theinterface modulepairIM 460-1 and IM 461-1 can only support one sender and one reciever, and that the maximum distance between the two is 1,5 m at the most. So it is designed for local (inside the panel) applications only; the supported module typesare also limited, as the K-bus is not supported on the dedicated interface. You can study this information (and much more)in chapter 6 of the following manual: http://support.automation.siemens.com/WW/view/en/1117740 Hope this helps, Daniel Chartier |
12/21/2008 1:09 PM | |
Posts: 2 Rating:
|
thanks Danial for your help....i understand now
marry christmas |
12/22/2008 1:54 PM | |
Joined: 4/24/2006 Last visit: 7/31/2025 Posts: 9027 Rating:
|
Hi Daniel, I think it's possible to connect two Expansion Racks The maximum distance between Sender and Receiver is 1,5 m. Best regards, Wizard |
Last edited by: Wizard at: 12/22/2008 1:59 PMLast edited by: Wizard at: 12/22/2008 1:55 PM |
|
Follow us on