7/4/2020 4:04 PM | |
Joined: 9/27/2006 Last visit: 9/17/2025 Posts: 12411 Rating:
|
Hello engineer; If you do not know the passwords to access the functions on your OP 37, and if you do not have a backup of the program (ProTool), you are locked out of the panel, basically. Unless the programmer left the Superuser standard login at its default value "100". A Superuser is allowed access to all functions of the panel, so if you are lucky enough to be recognized as superuser you could reset all the password values. Have a look at chapter 5 "Password Protection" in the following document. OP 27, OP 37 operator panels https://support.industry.siemens.com/cs/ww/en/view/1142800 Hope this helps, Daniel Chartier |
Follow us on