8/3/2020 4:35 PM | |
Joined: 6/4/2010 Last visit: 9/30/2024 Posts: 387 Rating:
|
Dear Milos, for the data sheet button to work you must do the following:
The code uses the value of the BIM property "<1.960/3L.00.8> Link (URL)" or "<CIBSE-1033.8.14> Product Literature [URL]" as URL. Please find a more detailed description with print screens in the attached word document. If the above procedure should not work, please contact the local Siemens support organization and provide the IFC file and a backup of the Desigo CC project, so that they can investigate. Best regards Albis AttachmentDataSheetButtonToWork.docx (395 Downloads) |
This contribution was helpful to
1 thankful Users |
8/4/2020 2:19 PM | |
Joined: 12/11/2019 Last visit: 6/22/2023 Posts: 18 Rating:
|
Thank you Albis. Still i can't manage to click on datasheet button. I created new project for testing, from Siemens CAD Browser for example picked 3 port valve and exported IFC file. Then in Desigo BIM Viewer imported that IFC file, but nothing changes when i click on model, datasheet button is still grey. I attached screenshots with steps what i did: 1. Siemens CAD Browser - picked 3 port valve 2. Export IFC file 3. Import IFC file in Desigo BIM Viewer 4. Screen without clicking on model 5. Screen when clicked on model So am i doing something wrong? Is this Siemens CAD Browser correct program to use for Desigo BIM? Best regards, Milos Milisavljevic AttachmentBIM datasheet problem.zip (346 Downloads) |
Follow us on