9/4/2020 2:15 PM | |
Posts: 8 Rating:
|
Hello,
I'm currently trying to connect the Simatic IOT2040 to Mindsphere. I do the onboarding with the help of elclipse / the description Documentation_SimaticIOT2000_MindsphereSiemens. https://support.industry.siemens.com/tf/ww/en/posts/how-to-use-mindconnect-lib-to-connect-the-iot2000-to-mindsphere/202603/?page=0&pageSize=10 # post806085 Everything works up to step 3.7 and I also have a connection between eclipse and the IOT2040. However, in step 3.8 (page 8) an error always occurs: Onboarding: MCL_COULD_NOT_CONNECT Does anyone have any idea why? I have two pictures attached Best regards! AttachmentBilder.zip (328 Downloads) |
9/18/2020 3:13 PM | |
Joined: 12/12/2016 Last visit: 7/25/2025 Posts: 640 Rating:
|
Hello, Would it be an option to use the mindconnect node in Node-Red? Best Regards! |
Follow us on