9/16/2020 6:48 PM | |
Joined: 7/21/2013 Last visit: 8/17/2025 Posts: 52 Rating:
|
Dear Expert I got problem when upgrade CPU to S7-1513-1PN and Sinamics G150 CU320 DP firmware 2.5. Because new PLC has no Profibus so I bought a new CBE20 (6SL3055-0AA00-2EB0) but I can not download new configuration (I mean can not update new topology). The fault and others info as attached file so could you please help me the solution how should I do now. Thank you very much Regards BN AttachmentG150.zip (234 Downloads) |
9/17/2020 7:09 PM | |
Joined: 10/11/2006 Last visit: 9/8/2025 Posts: 6039 Rating:
|
Hello, Hardware compatibillity of SINAMICS S120 Control Unit CU320-2 https://support.industry.siemens.com/cs/ww/en/view/44614547 CBE20 work with CU320 and CU320-2. During Power on the CBE get the firmware from the CU, and when it is finished you have to do a PowerOff/On. Please analyse your behavior with starter, to get the fault messages. |
With best regards, |
|
9/19/2020 10:09 AM | |
Joined: 7/21/2013 Last visit: 8/17/2025 Posts: 52 Rating:
|
Hello Sir After I installed the CBE into the CU320 and config the topology (CU configuration Wizard) select option board is CBE20 ... then download to CU320 but it's always tell me the illegal parameter then error download. Also it's fault, comparison topology different online/offline but I also can online with CU over the CBE20. I also can not find the parameter P8835 so how can I access this parameter Thank you very much Best regards B.N |
Follow us on