1/20/2009 10:32 AM | |
Joined: 10/15/2008 Last visit: 4/6/2022 Posts: 35 Rating:
|
Dear all: I have meet one problem. I use S7-315T CPU and S120 to control motor. But When I use function "MC_MoveRelative" tolet motor running, I observe one situation. Motor occur "overshooting" when it start and stop running. My speed setpoint value is 120 RPM, but actual speed value that it's over 120 rpm when motor start and stop running. Does here anyone can tell me which parameters in S120 can improve or adjust this situation? Attachmentovershoot_1.zip (509 Downloads) |
Follow us on