11/17/2020 11:17 AM | |
Joined: 4/23/2010 Last visit: 11/23/2024 Posts: 8092 Rating:
|
Hello, Depending upon motor power & application you need to select Sinamics drive. Next you need to check compatability of CU unit you have with drive module & then you run your motor with drive which operation can be controlled by CU. Please refer SINAMICS S120 Getting Started with the STARTER Commissioning Tool application example for more detail information. HTH |
Last edited by: Jen_Moderator at: 11/17/2020 13:38:27Optimized link. |
|
11/27/2020 5:47 AM | |
Joined: 5/12/2006 Last visit: 9/2/2025 Posts: 22709 Rating:
|
have you connect the 230v correctly? the messages mean that only the 24V available but not 230V on the Powermodule |
12/3/2020 8:01 AM | |
Joined: 4/23/2010 Last visit: 11/23/2024 Posts: 8092 Rating:
|
Hello, Please refer below application example. SINAMICS G/S: Speed control of a G120/S120 with S7-300/400 (STEP 7 V5) via PROFINET (PROFINET RT) Positioning a drive with standard telegram 9 SIMATIC S7-1500T: Control of a Multi-Carrier-System HTH |
Last edited by: Jen_Moderator at: 12/03/2020 10:56:41Optimized links. |
|
Follow us on