12/21/2020 7:07 AM | |
Joined: 12/2/2020 Last visit: 4/12/2024 Posts: 40 Rating:
|
Hello, I have a sinamics 210 with S7-1500 and I have some differences between setting and actual values. First of all, I make my tests without load on the motor shaft. For example I set speed "200" and I read actual speed: "60". Also I read for example actual torque "0.02" and set limit in TorqueLimiting function: "2". Thanks ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 12/21/2020 10:01:50New subject after splitting |
|
Follow us on