1/10/2021 6:09 PM | |
Joined: 6/7/2020 Last visit: 7/22/2025 Posts: 3 Rating:
|
i have the same problem with safety PLC ET200SP F (6es7 512-1sk01-0ab0 ) and communicate with S120 Drive when making online with the CPU, go in stop mode with the error in below i made trial change the communication load 15% , 20%, 30% ,40% , 50% and the same problem I changed the maximum cycle time of safety FOB_RTG1 OB123 from 120000 mic sec to 600000 and the same problem Error: Safety program: Maximum cycle time exceeded F-runtime group 1 Current cycle time of the F-runtime group 1: 1016000 µs PLC_EnamelL5 / PLC_EnamelL5. The current cycle time of the F-runtime group is greater than the configured "Maximum cycle time of the F-runtime group". Check the "Maximum cycle time of the F-runtime group" and the cycle time of the F-OB. Check whether test functions with the PG may have extended the cycle time. You can obtain more information by searching for the event ID in the STEP 7 online help. i made trial change the communication load 15% , 20%, 30% ,40% , 50% and the same problem I changed the maximum cycle time of safety FOB_RTG1 OB123 from 120000 mic sec to 600000 and the same problem I faced this problem when I start commissioning S120 i can configure 2 Axis with technology object this error from time to time but when I start config Axis 3, stop mode all the time ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 01/11/2021 09:39:30New subject after splitting |
|
Follow us on