1/21/2021 2:59 PM | |
Joined: 1/22/2018 Last visit: 5/27/2025 Posts: 31 Rating:
|
Hello, I have the same problem. Digital input are defined in the program as I1.0 - I3.7 and when i give +24V DC on input terminal, LED lights turn ON but the input in program isnt getting signal on I1.0 - I2.7, and on I3.0 - I3.7 im getting OK readings. And outputs are OK too. Anyone solved this problem? BR ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 01/22/2021 08:07:00New subject after splitting |
|
1/22/2021 11:44 AM | |
Joined: 1/21/2013 Last visit: 11/20/2024 Posts: 4620 Rating:
|
Hello, if you leave I124.0 as default, what happens? It works? |
1/30/2021 6:52 AM | |
Joined: 1/22/2018 Last visit: 5/27/2025 Posts: 31 Rating:
|
Hi, valbright39 and Ayman Elotaify thank you. You guys were right. I should connect terminal 1 (1L+) and then i get signal at input on terminals, like u guys said. It is shown on wiring diagram on module too. BR THOMPSONvk |
This contribution was helpful to
1 thankful Users |
Follow us on