3/14/2019 3:18 PM | |
Posts: 5 Rating:
|
Hi all i have a problem with my stama mc540/s machine with Siemens 840c control. the alarm is 3092 specified velocity too high , for 4 the and 5 the axis Respectively MAGAZINE MOTOR AND TOOL CHANGER MOTOR. can anyone help me identified the parameter. in jog mode both axis are ok and no alarms. this alarm comes only in MDA or AUTO. if I call any tool number magazine will come to the position but alarm will highlight immediately when the motor is moving. Please suggest ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 3/15/2019 8:41:41 AMNew subject after splitting |
|
3/15/2019 8:46 PM | |
Joined: 10/17/2007 Last visit: 8/29/2025 Posts: 4423 Rating:
|
The NC MD response for this alarm is 2802---Max speed (G0) But I suggest you don't change NC MD, you can reduce programmed speed for ATC motor and MAG motor--check they are in Sub -NC program attached alarm message
|
If you like my comments please |
|
3/18/2019 1:56 PM | |
Posts: 5 Rating:
|
Hi thanks for the suggestion. tool changer worked good. thank you very much |